Jimmek
- Total activity 22
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 2
- Subscriptions 6
Posts
Recent activity by Jimmek-
RealSense Camera Tripod Specifications Screw size for tripod legs
RealSense Camera Tripod Screw size for tripod legs, not the camera.
-
Syncing two D455 Cameras, one as master and one as slave unsuccessful
Cameras: two D455s S/N 037322251516 S/N 037322251668 FW: 5.12.09.00 SDK and Viewer 2.40.0 Win 10 PC New with Intel 7 CPU Been unable to get cameras to operate in sync master/slave mode. I ha...
-
Specs Regarding 1.8V External Sync
Documentation for using external sync for D455 cameras has the trigger voltage level as 1.8 V . What is the tolerance level for this 1.8V signal? Is the non-trigger state 0 volts and is there a t...
-
D455 configuration, saving, recording
From the RealSense viewer UI, various RGB, Stereo, Depth, and Tracking settings can be set by the user. Can all of these settings be saved to a file or files for later recall/loading/importing? Is...
-
Format structure of the D455 .bag file
Where can the format structure of the .bag file be found if I want to extract information directly, for example, where in the .bag file can IMU and/or trajectory be found.
-
Extracting IMU and trajectory data from D455
I use rs-convert to get PNG files, Metadata, and csv files for depth. Ex: rs-convert.exe -i name.bag -p testb -v testb which gets me all the PNG, metadata, and depth frames .csv files. How to I ...