Yzkzero

  • Total activity 14
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 0
  • Subscriptions 4

Posts

Recent activity by Yzkzero Recent activity Votes
  • Does D450 module has longer life-cycle than D455?

    Hi, We are going to use D455 in our product. But D455's life-cycle is too short for us (3 years as far as I know). So we wonder if D450 module can have longer life-cycle time as the module seems to...

  • Incorrect depth image by D455

    Hi, With the new D455, I noticed many times that the wrong depth images were generated. In the below screenshot, you can see the two different depth image took in same place. The upper one is wrong...

  • Right MIPI error

    Hi, I encountered "Right MIPI error" for several times with the new D455 camera. At first, I observed the bad depth image quality in my application. Then I switched to "Intel RealSense Viewer" and ...

  • Are intrinsicis always the same for same type of camera?

    For example, for two D415 cameras, do they have the exactly same intrinsic parameters by default? Or each of them have been calibrated in factory and hence have their own different intrinsic parame...