Yzkzero

  • Total activity 14
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 0
  • Subscriptions 4

Activity overview

Latest activity by Yzkzero
  • Yzkzero created a post,

    Does D450 module has longer life-cycle than D455?

    Hi, We are going to use D455 in our product. But D455's life-cycle is too short for us (3 years as far as I know). So we wonder if D450 module can have longer life-cycle time as the module seems to...

  • Yzkzero commented,

    Hi MartyG, I found a similar issue here: https://github.com/IntelRealSense/librealsense/issues/7777

  • Yzkzero commented,

    Thanks for the suggestion, but it does not work for my case. Because RGB is necessary to our project. Also turning off dot pattern will result in bad depth image in our scenario (ambient light is n...

  • Yzkzero commented,

    When the issue happens, disabling RGB can eliminate the issue. But I cannot say the issue never happens if RGB is disabled because the issue is sporadic and it will need much time to test. As far a...

  • Yzkzero commented,

    Hi MartyG, The hardware reset can only temporarily solve it and the issue will happen again later. Also it is not specific to using viewer, it also happened in my application using librealsense. An...

  • Yzkzero commented,

    Hi MartyG, Thanks for the quick reply. I know the strong light may saturate the sensor and cause the problem. But the issue also happens in a room without string light (I never took it outdoor). Ac...

  • Yzkzero commented,

    BTW, the issue is not always "shifting with band". Sometimes the depth image is totally mess up. And in any case, a hand waving into the camera view can make the depth back to normal...

  • Yzkzero created a post,

    Incorrect depth image by D455

    Hi, With the new D455, I noticed many times that the wrong depth images were generated. In the below screenshot, you can see the two different depth image took in same place. The upper one is wrong...

  • Yzkzero created a post,

    Right MIPI error

    Hi, I encountered "Right MIPI error" for several times with the new D455 camera. At first, I observed the bad depth image quality in my application. Then I switched to "Intel RealSense Viewer" and ...

  • Yzkzero created a post,

    Are intrinsicis always the same for same type of camera?

    For example, for two D415 cameras, do they have the exactly same intrinsic parameters by default? Or each of them have been calibrated in factory and hence have their own different intrinsic parame...