David Thevenin

  • Total activity 7
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 0
  • Subscriptions 1

Activity overview

Latest activity by David Thevenin
  • David Thevenin commented,

    Hi JesusI do not have PC, only Macs. I do consider Linux into a Virtual Machine, but it looks to me a bit complicated. I'm evaluating the solution tho. But for now I'm still considering to return t...

  • David Thevenin commented,

    Hi Jesus I understand; thanks for the investigation and the summary. I did test on a fresh installed macOS, means that  kextstat | grep -v apple return nothing, and it does not work too.   Anyway, ...

  • David Thevenin commented,

    Hi Jesus Thanks. If it can help, I could test the pull request on my Mac. Bests David

  • David Thevenin commented,

    Hi Jesus Garcia Do you have update on that issue?Because of this bug, I can't use the cameras on MacOS; it's blocking. In the time being I could down grade to a previous version of the SDK for inst...

  • David Thevenin commented,

    Thanks  here more information related to the installation: macOS       10.57.7libusb          1.0.23pkg-config   0.29.2_3glfw             3.3.2 Regards

  • David Thevenin created a post,

    EXC_BAD_ACCESS On MacOS

    Hi I just received my L515 camera and I'm trying to run some code examples on MacOS. For instance I'm able to compile rs-hello-realsense, but when it comes to run the example I have an exception EX...