Vinicius Ramalho
- Total activity 6
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 2
Activity overview
Latest activity by Vinicius Ramalho-
Vinicius Ramalho commented,
Thanks MartyG, We managed to find and buy the interposer PCB and it seems that the issue was solved. D450 and D435 DO need different interposer cables.
-
Vinicius Ramalho created a post,
D450 modules are being recognized as D430i
History: We bought the D450 modules pack, however, the flat cables to connect the image sensors board to the depth processor board did not came together, and neither did the USB-C cables (But that ...
-
Vinicius Ramalho commented,
Thanks for responding MartyG. I did run the calibration tool (Not the dynamic calibration) and it said that the calibration was good, i'll try the dynamic calibration tool as well as changing the d...
-
Vinicius Ramalho created a post,
Accuracy with sunlight noise
I used 2 D435 cameras in a outdoor application (between 2~4 m), but a lot of wavy noise was detected. So, i did some captures comparing indoor scene and indoor scene with sunlight (to simulate a ou...