Aznie Syaarriehaah
- Total activity 121
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 46
Comments
Recent activity by Aznie Syaarriehaah-
Official comment Hi Bettychanlh,Yes, the box comes with a USB C cable. The camera cannot be converted to a network device by using the USB C to RJ45 adapter. These adapters are used on laptops and tablets where the...
-
Hi Suleman, The DIM Weight Software SDK is based on C++ so if you want to use it with a C# program you will have to write a wrapper for it. However, the L515 can be programmed using the Intel RealS...
-
Hi Hamiddreza Alidousti, The D415 and T256 connection to Raspberry Pi 4 was never validated from our side. However, there is a Whitepaper Intel® RealSense™ Tracking Camera T265 and Intel® RealSen...
-
Hi Juergen Poesel,Thank you for contacting us.We handle this issue via a private ticket.Regards,AznieIntel RealSense Customer Support
-
Hi Wonhee,Thanks for reaching out to us.Yes, you’re right. L515 is being discontinued as of February 2022.The suggested alternatives for L515 are D455 and D435i.Please visit the following page for ...
-
Hi Smartdome, We handle this issue via a private ticket.Regards,AznieIntel RealSense Customer Support
-
Hi Yamadas603, Thank you for contacting us.We handle this issue via a private ticket. Regards, Aznie Intel RealSense Customer Support
-
Hi Smartdome, Can you share the screenshot of your Device Manager with the camera nodes expanded as shown in the picture attached? Regards, Aznie Intel RealSense Customer Support
-
Hi Min1003k, We handle this issue via a private ticket. Regards, Aznie Intel RealSense Customer Support
-
Hi Min1003k, Can you test the camera on another computer and see if the same issue arises? Regards, Aznie Intel RealSense Customer Support