Pavel Stoffel
- Total activity 8
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 1
Activity overview
Latest activity by Pavel Stoffel-
Pavel Stoffel commented,
Hi Marty, I've been a software developer in the Silicon Valley for over 30 years. I've always shied away from contacting customer support from any company. My impression has always been that suppor...
-
Pavel Stoffel commented,
Hi Marty, Your last advice fixed my problem: "the next fix you could try is to go to each of the two drivers in Device Manager, right-click on them and select Uninstall. When both drivers are remo...
-
Pavel Stoffel commented,
Thanks, and Good Night
-
Pavel Stoffel commented,
Hi Again, My Windows 10 is real weird. It is an enterprise version. I wonder if the IT department messed with it. Went to Troubleshooting: "Hardware and Devices" was not an option: Scrolled all...
-
Pavel Stoffel commented,
Marty, As you can see from my Device Manager above: The 415 camera appear ONLY under USB devices. I checked: they do NOT appear under Cameras. When I go to Windows Settings, I do not get the opt...
-
Pavel Stoffel commented,
Hello Marty, Yes, I downloaded and installed the full 791 mb RealSense SDK using the Intel.RealSense.SDK-WIN10-2.36.0.2034.exe file from Assets. I get the same results: Windows Device Manager sees...
-
Pavel Stoffel created a post,
D415: there are no connected devices
My device: My OS: From my Device Manager: From FW Update Manger: Why cannot the update manager see the D415 camera? Tried all four USB ports on the Lenovo ThinkPad computer. The RealSense Vie...