Kent Liew
- Total activity 8
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 3
Posts
Recent activity by Kent Liew-
Part Number (with USB type C cable)
What is the ordering part number for the part numbers mentioned below that come together with USB type C cable? I believe that the part numbers in below are without the cable. 1) PN#82635ASRCDVKHV ...
-
82635ASRCDVKMP
My customer feedback that they received the PN#82635ASRCDVKMP (Real Sense Depth Camera D415, 30 pack) without the USB type C cable available inside the package. Therefore, if the cable need to orde...
-
Intel RealSense Depth Camera D415
Hello, May I know the Intel RealSense Depth Camera D415 will include USB cable or not? What is the cable length? Also, can Intel provide the 3 meter length USB cable for this part when I order it? ...