Lghasemz
- Total activity 44
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 8
- Subscriptions 3
Comments
Recent activity by Lghasemz-
I understand :) Thank you very much
-
5) that is correct about power output but as the last question: from question 5 I meant, If we put the camera in a constant location (150cm from the object), and put the external illuminator nearer...
-
Thank you very much, 2) we purchased D435i but can not use it in our project since it produces dots on the stream (we have discussed this issue previously), so assume that we use the SR300, and the...
-
Hello Marty, I had read somewhere in an official document regarding the Infrared impacts to human, but I cannot remember the source and the conclusion. 1) In general, is Infrared dangerous for huma...
-
It worked, Thank you so much.
-
Hello Marty, Hope you are fine. I got an update notification and I confirmed to update, but after update the streams are not working. What should I do?
-
1) Yes the IR stream continues streaming frames (the camera still works) but doesn't behave like usual IR. With my partial knowledge IR should transparent sunglasses (940nm) and work in darkness (g...
-
Hello Marty, I have two questions, One regarding the second screenshot from my previous message, the other about external IR illumination. 1) In my previous message, I sent you the comparison betwe...
-
Thank you for the links. Regarding those scattered dots: I remember from our previous talk when we asked about how we can increase the range and the quality of the IR stream of the SR300, and you s...
-
Hello Marty, Hope you are fine. Finally we received our D435i. 1) we want to record/save the streams as pm4 not bag. Is there a way to do so? For our previous experiments with SR300 we simply recor...