Sheethal Ng
- Total activity 26
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 5
Comments
Recent activity by Sheethal Ng-
Hi Marty Here is my requirement 1. Initially the IR emitter will be turned off 2. I need to then turn on the emitter and get depth frame 3. Turn off the emitter and get IR frame I believe when we...
-
Even if the values in npy are just distance of pixels, is it possible to get a depth image
-
Can I use the depth data(distance data) and get a 2D depth image
-
Python npy file.
-
Hi Marty, I have dumped the distance of each pixel for the entire frame. Is it possible to get a depth image using this data??
-
-
Hi Marty, I placed two objects of different size at different known distances facing the center of the camera and compared with the depth distance obtained from the python wrapper. My problem is...
-
The above image is an IR image captured with following configuration 1. Resolution (1280x720) 2. FPS 6 3. IR emitter off 4. Format y8 Below is the result in format (x,y,distance) 4 273 11.0350...
-
My question is after dumping the data how do i know the distance of each pixel is correct.
-
Suppose if i dump the depth data using the above approach for one frame, how do i verify the dumped data is correct