201990202
- Total activity 6
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 2
- Subscriptions 1
Activity overview
Latest activity by 201990202-
201990202 commented,
MartyX Grover, Thank you so much for the prompt response. I will follow the provided links.
-
201990202 commented,
Furthermore, can I use the USB-C port on the camera for streaming? Does the camera need a dedicated 12V power supply to work? If yes, how can the power supply be connected without using the GMSL/FA...
-
201990202 created a post,
De-serializer Board
Good day. I have a D457 realsense camera, unfortunately, it's been very challenging to get it to work. The first problem is the additional hardware(components) required such as the deserializer/ada...