George

  • Total activity 9
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 1
  • Subscriptions 1

Activity overview

Latest activity by George
  • George commented,

    thanks, after going through the sign up and sign in for GitHub I was able to leave a "feature selection Issue #6365." Hope that's what you meant.

  • George commented,

    Upgraded to Skype 8.59. Can now select Depth, Virtual or RGB. Depth gives the green monster still on the screen shown in the above comment. Virtual gives the same kind of picture as above. RGB is a...

  • George commented,

    I'm using business Skype ver 8.56.0.102 - only allows the virtual camera selection and RGB is the view that appears, just like you said. But when I'm in a skype session with someone the image is no...

  • George commented,

    Both settings in windows are on. The troubleshooter does not have a feature for the camera

  • George commented,

    don't have a way to select virtual driver. The only item in the dropdown by camera is RealSense 3D camera  

  • George commented,

    The only entry beside CAMERA as you describe is Intel(R) RealSense(TM) 3D Camera Virtual Driver. In Device Manager I tried update driver and am informed the latest version is installed. In properti...

  • George created a post,

    Default driver

    RealSense Front F200 camera factory installed in desktop running Windows 10. Using Skype or Zoom, image is a green "monster". In Zoom I can change from the Depth driver to RGB and get a real image....