Scott Stevens
- Total activity 5
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 1
Comments
Recent activity by Scott Stevens-
In considering a powered hub how much power will each Realsense draw? For example - the AmazonBasics hub provides 1 port with 1.4amps; and the others with 900mA each; a max total of 4A. The reason ...
-
FYI - on the computer with the 2 D435s - I lost all connections to the cameras. I unplugged-replugged the USB cable at the computer numerous time, no help. I downloaded a slightly newer version o...
-
MartyG thanks for the reply. Will 'any' powered USB3 hub work? see image
-
I'm having similar issues on multiple machines. I have 12 Windows 10 machines with a D435 camera & Leap Motion attached. Each time we boot up the group of computers 1-4 of them don't recognize t...