Kyuman Lee

  • Total activity 11
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 2
  • Subscriptions 3

Posts

Recent activity by Kyuman Lee Recent activity Votes
  • Change a wide FOV RGB camera to the D430 module

    Is there any reason why the FOV of the RGB camera on the D430 module is smaller than the FOV of the IR camera on the D430 module? Can I change a wide FOV (similar to or larger than the FOV of the I...

  • Wrong Pose Estimates of T265

    1. When using a T265 + ROS Wrapper indoors (static environment), the following three problems often occur. These happen even when only a T265 is used in the Viewer.- Under estimate: Estimated too l...

  • Multiple Camera Support of D4 VPU / RGB Calibration on D430 Module

    1. When changing a custom RGB camera on an Intel D430 module, is it possible to set the intrinsic & extrinsic parameters of the RGB camera? If possible, where and how? Is it possible only on the CP...