Scap

  • Total activity 19
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 0
  • Subscriptions 1

Comments

Recent activity by Scap Recent activity Votes
  • Thank you very much for your assistance! I look forward to continuing.   for simplicity I have added a realsense user.       Is there a specific version of realsense-viewer I should be using on my...

  • I am indeed using putty, I understood the initial username being "realsense" was due to the configuration on the raspberry pi image. As I setup the ubuntu machine from scratch my username and passw...

  • I can ssh into the ubuntu computer from my windows host, but the ubuntu computer does not have a file at `/etc/dhcpcd.conf` as I believe that is a file typically on raspberry pi's. I did however se...

  • Sorry, I was updating my previous post before I realised you had answered about the manual installation of udev rules. Udev rules have been installed. Realsense-viewer output is attached at the end...

  • OK, after retrying in a clean directory it has succeeded.  Running realsense viewer does show the camera connected via USB3.2 and I can stream over USB via the application. Should it be possible to...

  • OK, so I shall build with the options of: -DFORCE_RSUSB_BACKEND=true -DBUILD_NETWORK_DEVICE=ON For information I will be building on a fresh install of ubuntu 18.04 LTS. Should I follow the instruc...

  • Thank you for the response Marty! I have been compiling many versions and trying many kernel / driver/ firmware / SDK combinations to no avail. Is there a combination of OS, Kernel, SDK (2.51.1) an...