Thomas Chenus33
- Total activity 71
- Last activity
- Member since
- Following 1 user
- Followed by 0 users
- Votes 0
- Subscriptions 6
Comments
Recent activity by Thomas Chenus33-
No, I didn't change anything about that part. It's since I switched to the server with the win7 SDK and the associated DLL that it doesn't work anymore !
-
Yes, I know. But precisely this doesn't work anymore, because it doesn't recognize the ThreasholdFilter function anymore! I think it doesn't exist in this version or is called differently. Because ...
-
And for the ThresholdFilter do you have an idea ? Because with this filter I can change the min/max value of depth, and it's realy important for my project ...
-
The good way to write this with the win7 DLL is : Thanks for the link :)
-
Hello Marty, I went back to the Intel.Realsense.dll, like I told you 8 messages ago. I think it's the one that should be executed in my program as I'm on a win7 SDK. As you can see in the screen sh...
-
Ok thanks Marty, I'm stuck with the server for now, I'm waiting for Jesus Garcia's answer. I hope you can help me Jesus :)
-
The goal is to make the camera communicate with the program of a robot running on the server, today I don't have a computer for the robot but only these servers. I'd like to succeed without having ...
-
Yes, he doesn't know those instructions anymore! Like it doesn't exist in Intel.Realsense.dll. But I checked and I used IntelRealSensed.dll before and it worked. So I came back as before with this ...
-
And yes before realsense2.dll and Intel.RealSensed.dll was in the Debug folder
-
Yes. But here I just put Intel.Realsense.dll (it's good syntax, not Intel.RealSense.dll or Intel.RealSensed.dll) which was in the same directory as realsense2.dll I don't know if this should fix my...