Martin Studer
- Total activity 19
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 6
Posts
Recent activity by Martin Studer-
Problems with the depth image on the Raspberry Pi 4
Dear Community, I am using the D435 with a Raspberry Pi 4 and CV2.Everything has been working well so far.Then I had to replace a circuit board in one of the cameras, and since then the depth image...
-
Object detection ending after 4h with this failure...
Hello Community I use the Camera D435 with a RasperryPi 4, 4GB RAM and an SD card with 32GB.The camera detects objects and simultaneously measures the distance. Is an object closer than e.g. 4m swi...
-
Object detection
Hi Realsense-Team I want my camera that runs with object recognition on a Raspberry 4 to only recognize some objects and not all.I found the following program line in a file: CLASSES = ["backgr...
-
Error: ImportError: No module named pyrealsense2
I followed all instructions and read and tried everything that has already been written about it in the forum.But I just can't get any further.I'm almost desperate. I would like to test the rs-hi-r...
-
Example Code only in C/C++ how I can use for Python?
Hello communityI have installed the RealSense SDK2.0 software on the Raspberry and it also runs.Now I wanted to run the Hello-Realsense program.Which compiler / software do I have to use on the Ras...
-
No Code in this example
Dear Intel-Team On your Website: https://dev.intelrealsense.com/docs/code-samples you have code examples. But in this folder: Here is no content, when I open it. It is possible to fill t...