Dapeng Zhang

  • Total activity 4
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 0
  • Subscriptions 1

Activity overview

Latest activity by Dapeng Zhang
  • Dapeng Zhang commented,

    So far, no one is interested in or wants to answer this question. Could someone help? Feature detection and landmarks are in the white paper of T265:        https://dev.intelrealsense.com/docs/inte...

  • Dapeng Zhang commented,

    Thanks. here is the link https://github.com/IntelRealSense/librealsense/issues/5909

  • Dapeng Zhang created a post,

    T265 vslam with landmarks and relocalization

    I'm extensively testing T265 and its v-slam. The testing is done on a floor of 20m x 30m with several rooms. Height changes are ignored. T265 is attached to the top of a helmet, shooting towards ce...