Lukas Faschingleitner
- Total activity 4
- Last activity
- Member since
- Following 1 user
- Followed by 0 users
- Votes 0
- Subscriptions 1
Activity overview
Latest activity by Lukas Faschingleitner-
Lukas Faschingleitner commented,
As already mentioned we don't need to get closer to the object. We need a way to get the depth information of the in the picture marked area. Only of this area! Which parameters or settings in th...
-
Lukas Faschingleitner commented,
We have the D415 model.In the link you mentioned, there are only examples of objects with a high range. Our camera is less than 50 cm away from our object and the notches are less than 1 cm deep. I...
-
Lukas Faschingleitner created a post,
how do we get a result like in this picture?
We got this model with the default parameters of the itSeez3D-Software. How do we get a similar result in the Software "RealSense-Viewer"? The object, that is represented, is a concrete slab with ...