Johannes Rabe

  • Total activity 8
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 1
  • Subscriptions 2

Activity overview

Latest activity by Johannes Rabe
  • Johannes Rabe commented,

    Hi MartyX Grover,    thank you for the quick feedback and the hint on IR interference. I feel like we may need additional information, but may need some alignment first before applying for an NDA.

  • Johannes Rabe created a post,

    Eye-safety with other emitters

    Hi, I found the documentation that Realsense D400 series is eye-safe as Class 1 Laser product following IEC 60825. Few requests in this support portal also refer to this, e.g. https://support.reals...

  • Johannes Rabe commented,

    Hello MartyG, from the tests we did so far, it seems that the triggering/synchronization works fine now. Thank you for your help.

  • Johannes Rabe commented,

    Hi MartyX Grover, thank you very much for your response!   These are two very valuable points: 1) I tried to get to as close as possible to 30 Hz (which my scope self-measures at 30.000000169... Hz...

  • Johannes Rabe created a post,

    Issue with triggering D435 with external trigger

    Hello, I have a Realsense a few D435if and would like to trigger them with a trigger generated by an external device. I made connecting cables following the description in https://dev.intelrealsens...