Simon
- Total activity 9
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 1
Comments
Recent activity by Simon-
Hi james, well I'm also a bit disapointed but finally i find a solution (that is ok for my application). The problem seems to be on the windows side (the kernel if i remember well), so unstability ...
-
if I retry to install the recommanded firmwar, i have this error (the error is in french with weird caracter sometimes): Started Firmware Update processBacking-up camera flash memory ERROR: Backend...
-
I can upgrade the firmware with the rs-fw-update.exe with the terminal. That's what I've done earlier and the viewer tell me that the camer is running with 5.11.15.0 firmware when I click on Info b...
-
I just tried now all my 3 usb port (2ports are 3.2 and 1 is 2.1) and that's working for 1 seconde each time I change the port but it still finish to stop sending frame
-
I just tried now, It don't change something. Just after that, when I try to activate the rgb camera, i have an error message which is "the profile is unsupported". The preset which is automatical...
-
I use the one that came with the camera. I also tried to reduce the fps and resolution to the lowest as possible but nothing change
-
well now i'have successed to update the camera using this tutorial: https://dev.intelrealsense.com/docs/firmware-update-tool so now my d435 run the 5.11.15.00 firmware. But i still cannot see more ...