Ramesh
- Total activity 14
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 1
Comments
Recent activity by Ramesh-
Okay. Thanks for that.
-
I have filed the driver crash issue on github. https://github.com/IntelRealSense/librealsense/issues/5076 I still haven't got a response. The issue is critical to us. Is there a way to escalate it ...
-
I don't see any logs being generated which is confusing. Am I missing something? I will file the driver issue on Github as well.
-
If I'm logging firmware, it has to be alongside our app, so that we can see the sequence of events. Also since OpenNi2 wrapper is being used, it would be necessary to check if everything is alright...
-
I built the debug drivers with symbols and was able to get a better view of the call stack.
-
Okay. I'll look into those options. I'm aware of the 10-port hub, but I'm concerned whether the single hub will be able to handle the bandwidth. Also power stability of port is what I think was the...
-
We are trying now with the newnex cables and using powered usb3 hubs(4 Transcend hubs with 3 cams connected and leaving one port free on each). The system is a lot better now, as in very less conne...
-
Okay, that makes sense. So getting the port quality up to par would be extremely important in that case. Could you comment on the two other "active" options I'm considering? I have been considering...
-
I agree that high-wattage PSU solely won't fix the power instability issue at the USB port, but I wanted to point out that in addition to that, the PCI cards we are using are of high quality and th...
-
I tried upgrading to the Newnex cables. With this new setup I'm observing frequent connect/disconnect with the cameras. In the Realsense viewer app, the connection shows up as USB 3.2, so I believe...