Yasser

  • Total activity 5
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 0
  • Subscriptions 1

Comments

Recent activity by Yasser Recent activity Votes
  • As you correctly understood, we don't actually need a Camera set up as master. I was simply planning on replicating the pulse from one as the multiple camera guide (https://dev.intelrealsense.com/d...

  • Ok, so if I understand it correctly. We would need to perform the following steps: Set up a camera as master with the exact setup we want to use, including exposure time, fps etc. Connect the trig...

  • Thanks for the quick answer. I could definitely splice it but if I had 1.8V available on one of the pins then I would have used a step down board so was just wondering if one of the other pins had ...