Yasser
- Total activity 5
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 1
Activity overview
Latest activity by Yasser-
Yasser commented,
As you correctly understood, we don't actually need a Camera set up as master. I was simply planning on replicating the pulse from one as the multiple camera guide (https://dev.intelrealsense.com/d...
-
Yasser commented,
Ok, so if I understand it correctly. We would need to perform the following steps: Set up a camera as master with the exact setup we want to use, including exposure time, fps etc. Connect the trig...
-
Yasser commented,
Thanks for the quick answer. I could definitely splice it but if I had 1.8V available on one of the pins then I would have used a step down board so was just wondering if one of the other pins had ...
-
Yasser created a post,
External hardware sync
We are planning synchronizing a D435 to a global time sync by using the external hardware sync from a Jetson TX2. As I understood, this would require a 1.8v signal kept high for 100us. So a couple ...