T Michals
- Total activity 8
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 3
Activity overview
Latest activity by T Michals-
T Michals commented,
If not follow jetsonhacks on youtube for a nano...it will work on TX2. Jim has not updated the build scripts for the TX2(except the TX2 flash) so you can use the nano scripts1) Flash TX2 2) Install...
-
T Michals created a post,
Trying to use ROS and rtmb and getting build error when installing rtmb
Required Info Camera Model T265 Firmware Version RealSense ROS Operating System & Version Ubuntu 18.04 LTS Kernel Version (Linux Only) Linux 4.9.140-tegra aarch64 Platform NVIDIA J...
-
T Michals commented,
Yes, I am/was using the d435 and t265 together at the same time on my USB hub (with no USB hub power adapter, strictly using USB power from TX2 ). I also am/was powering my mouse and keyboard on ...
-
T Michals commented,
You have to build the RealSense SDK with TM2 (BUILD_WITH_TM2 is ON) . https://dev.intelrealsense.com/docs/build-configuration . JetsonHacks explains but does not include this in his build on ...
-
T Michals created a post,
Does having the T265 cover not having the IMU in the d435
I have the d435 camera without the IMU. I also have the T265 camera. I am starting to learn how to program with ROS. What would be the short comings of not having the d435i (with the IMU), when it ...