Dobariyanikunj4

  • Total activity 5
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 0
  • Subscriptions 1

Activity overview

Latest activity by Dobariyanikunj4
  • Dobariyanikunj4 commented,

    small question: RGB sensor has zero distortions coeficient in factory calibration, means it is already rectified image. so, how intel perform factory calibration before user purchase?

  • Dobariyanikunj4 commented,

    @MartyG I have done calibration using that tool, but in result it gives RGB sensor has zero distortions. so, maybe default calibration is good. is recalibration must or can I use alos without recal...

  • Dobariyanikunj4 commented,

    @MartyG My camera has not drop or got hard knock. So, can I use RGB image taken from camera without doing calibration again?  

  • Dobariyanikunj4 created a post,

    is default camera calibration reliable?

    Hello,   I have intel realsense D435. As stated in intel realsense site camera calibration is not required for this camera because it is factory calibrated and also has zero distortion coefficients...