Shlane
- Total activity 5
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 1
Activity overview
Latest activity by Shlane-
Shlane commented,
We finally got the system to detect the Realsense camera. This was accomplished by first uninstalling and removing all the current and previous Realsense software installed on the machine, then w...
-
Shlane commented,
We had previously installed the latest version of the SDK 2.0 (build 2.24.0) but it doesn't make a difference. Is there any other way to separately install the T265 Windows10 device driver?
-
Shlane commented,
Marty, Thanks for the quick response. The T265 is not plugged into a hub (plugs directly into the the usb3.0 port on the front of the dell box. We have tried rebooting the dell box as you have sug...
-
Shlane created a post,
T265 Device not detected
We have confirmed that the T265 is plugged into a USB 3.0 port on the Dell Precision 7910 machine, however the T265 never shows up in the Windows 10 device manager After running the Intel Realse...