Rsharma2
- Total activity 8
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 2
- Subscriptions 2
Posts
Recent activity by Rsharma2-
Regarding D415 Calibration in Vertical Direction
Hi, I wanted to scan the D415 placed vertically to utilise the lesser Horizontal FOV from LIPScan, that is, I wanted to turn the camera vertically and then calibrate it for accurate measurement. Ho...
-
Regarding D435 Object Scanning Limitations
Hi, I'm trying to 3-D scan an object of size approx. 10cm * 10cm * 3cm which is circular symmetric using a turntable. The software which I've been using for this is RecFusion. I had two questions: ...