Antoine Triaux
- Total activity 18
- Last activity
- Member since
- Following 0 users
- Followed by 0 users
- Votes 0
- Subscriptions 2
Comments
Recent activity by Antoine Triaux-
thank you i will definitely try that Is there a way to get the confidence accuracy level of coordinates?
-
Hello MartyG, Using a polarizing filter helped a log with reflective surfaces. We are still getting the occasionnal misreadings though. Is there a way to identify the camera measurement(s) is/are n...
-
Is there anything that can be done to mitigate this issue?
-
this is the front view camera is pointing down at the ground, it is tilted about 25° from the horizontal plane i do not think the point cloud is distorted in any way? The points that are an is...
-
yes correct they both have filters
-
yes thank you, I forgot to mention that we did add a polarizer due to previous issues with reflective floors the image of the left IR receiver i posted in my first post is glare free
-
yes they are you can see the glare off of the tiles to the back of the image, closest to the windows
-
Yes MartyG that is correct, D435
-
Hello MartyG, I am looking for some more information. I ran a D415 for 3 hours yesterday at 26° room temperature, realsense viewer reported asic temperature to be 41°, IR projector temperature was ...
-
this is what I was afraid, I think with our case use we reach the limits of what the camera was intented for. We will definitely have to take precautions mounting the camera, mechanically speaking ...