Satsuna1352

  • Total activity 24
  • Last activity
  • Member since
  • Following 0 users
  • Followed by 0 users
  • Votes 0
  • Subscriptions 5

Posts

Recent activity by Satsuna1352 Recent activity Votes
  • Strange FPS when enable both color and depth streams

    Hello, my camera is D435 and I use python wrapper. I want to stream both color and depth in 60fps,  I close auto exposure and set the exposure value to 78.(I think it means exposure time=7.8ms) I r...

  • Align color and depth images

    Hi, I'm using D435 and python wrapper. I want to align depth to color image in 60fps, but when I use the align function(5th and 8th line), the fps drops to about 20, if I don't align them, the fps ...

  • Deproject pixel to point problem

    Hello, I have two questions. My camera is D435, and I have the need to calculate the angle between two vectors. Both my resolution of color and depth image are 640*480, and I've aligned the depth f...

  • D435 get timestamp of each frame

    I mainly use the Python API (Pyrealsense2) I have the need to get the timestamp of each frame caught by camera. The API provides a way to get timestamp: frames.get_timestamp() (frames = pyrealsense...

  • Recording Video in 60fps with threading and queue (Python)

    Hello, my camera is Realsense D435. I asked how to get 60fps RGB video stream before. Now I want to record the RGB stream into a video, but I want to separate the step of getting RGB image and the ...