MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Is Fixed Frame set to camera_link in RViz like in the image below?
-
Hi Javier Whilst Intel cannot comment on possible future RealSense products, you can be assured that the RealSense product range is continuing and the RealSense SDK continues to be actively develo...
-
You will need to add the command to the roslaunch instruction every time unless you edit the rs_camera.launch file to change the pointcloud_texture_stream line from RS2_STREAM_COLOR to RS2_STREAM_A...
-
Hi Sohwa427 Does your pointcloud become untextured if you add the command below to your roslaunch instruction, please? pointcloud_texture_stream:=RS2_STREAM_ANY
-
You are very welcome. I'm pleased that I was able to help. :)
-
The term 'virtual camera' refers to how the software-device interface can be used to define a pretend camera in software that is treated as though a real physical camera is attached. RealSense ca...
-
If you need to import depth frames from a non-RealSense camera into the RealSense SDK instead of RGB, as your mention of a stereo camera suggests, then you may be able to do so by reading the frame...
-
Hi Mikesaliphone The RealSense SDK has a concept called the Platform Camera by which non-RealSense cameras such as webcams can be identified and accessed. The easiest way to test it is by attempt...
-
There is not anything else that I can suggest unfortunately as use of Kinect cameras with the RealSense SDK / Viewer is not supported and the above link is the only reference to this error. I do a...
-
Intel can only provide support for its own RealSense cameras. In regard to the HResult 0xc00d36e6 error though, it has previously occurred with a RealSense camera in a case that was related to ...