MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
1. No, there is not a built-in Medium Accuracy preset. Medium Density fulfils that role. Of the other Presets available, I would recommend trying Default to see whether it meets your needs. 2....
-
Hi Toni Divic It would be possible to create a custom preset file in the RealSense Viewer tool by selecting Medium Accuracy, tweaking Viewer settings and then exporting the adjustments to a new pr...
-
Thank you for the additional information. What is the computer / computing device that you are running the Viewer and RealSense programs on, please?
-
Which firmware driver version is installed in your camera, please? You can find this information by clicking on the Info button near the top of the RealSense Viewer's options side-panel. If your...
-
-
Hi Eguenay There is not a need for a D455if model (the i refers to a RealSense camera equipped with an IMU component). This is because the basic D455 model was launched with an IMU in it. So if ...
-
Hi Horizon Zry The D455-class of cameras such as D456 would be suited for a minimum distance of 0.5 meters (50 cm). A D435 could meet your requirement of a 30 cm minimum distance. If you need ...
-
I do not think that initialize_rs being called more than once and looping, otherwise there would be an error if the pipeline was attempted to be started when it was already active. If depth stops...
-
When the images are blinking / flickering in HDR mode, you can stop it by configuring post-processing filter settings using instructions at the link below. https://github.com/IntelRealSense/libreal...
-
I suspect that the less than optimal RealSense depth image is mainly due to a phenomenon called repetitive pattern, where repeating horizontal or vertical arrangements of similar looking objects ca...