MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
RealSense cameras require high quality USB cables like the ones usually supplied with models such as D435i. This is because RealSense cameras can transfer high volumes of camera data, so they need...
-
Hi Maxime Ambard Thanks very much for your questions. 1. Yes, the HSF interposer cables - available in the official RealSense Store - will connect the Vision Processor D4 Board to your D430 board...
-
The frequency of the lights (and hence the Power Line Frequency that should be matched with it) typically depends on the country that the lights are in. North American regions use 60 Hz and Europe...
-
Hi Huangxunheu Pages 86-87 of the data sheet document for the RealSense 400 Series cameras provide information regarding how the FOV is calculated. https://dev.intelrealsense.com/docs/intel-realse...
-
Hi Alberto Barrio The RealSense Viewer tool has a calibration function called Tare for improving depth accuracy. It can be accessed from the drop-down menu of the More option near the top of the ...
-
Hi Aleks Loushkin Are any of the USB cables that you have tested with the official 1 meter USB cable supplied with the camera, please, or are you using cables that you purchased yourself?
-
Please disregard the above comment. It is an AI-generated advert.
-
Finally, sincere apologies for the multiple comments. This forum site's spam filter was blocking some parts of my reply from being posted, so I had to split it into parts.
-
Whilst the exposure and FPS values can be used to compensate for interference caused by fluorescent lights such as overhead ceiling strip-lights, it is easier to negate that interference by configu...
-