MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
If camera age was a factor then it is likely that the RealSense Viewer image would be negatively affected too. Does the depth data in the bag file still flicker if you play the file back in the V...
-
Hi Jashmehta The RealSense Viewer tool applies a range of post-processing filters to depth data by default and these can improve the quality and stability of the data. The effects of these filter...
-
It is unusual that two cameras would be experiencing the same problem. There are rare occasions when this 'No Frames Received' problem with the depth stream can occur if RealSense cameras have bee...
-
Have you ever been able to stream depth successfully since you purchased these two cameras or did the cameras work normally for a time and then develop this problem later? If the cameras did init...
-
There is an alternative method to the CustomRW gold reset that can be performed in the RealSense Viewer using the instructions at the link below. Do you still get No Frames Received from the depth...
-
Thanks very much for the images. Can depth data be displayed if you change the depth resolution in the RealSense Viewer from the default 848x480 to another resolution such as 640x480 or 1280x720
-
Hi Harshith Ylbf52 Yes, you can use an external signal generator (an oscilloscope, for example) to produce a trigger signal. It is difficult to implement though, as the frequency of the generated...
-
You are very welcome. I'm pleased that I could help!
-
Hi Dimouzoi Instead of stitching together multiple individual views, it will be easiest if you move the camera around the room in real-time to build up a scan. If you have a Windows computer then...
-
Thanks very much for the clarification provided by the link. In the earlier drawings it looked as though it represented the camera FOV being pointed at a flat board object. Apologies for the misu...