MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
If you use the 'RGB from left infrared sensor' RGB mode then it should perfectly align with the depth image as the infrared RGB image and the depth image are both originating from the left-side IR ...
-
3. Yes, the left and right IR sensors on the D455 camera model have an FOV size that is 75 degrees wide in the horizontal, as shown on your diagram. 4. If an object was half in and half out of ...
-
Hi Bitxuyang RealSense 400 Series cameras such as D435i are Active Stereo. Structured Light is a different camera technology. The older retired SR300 RealSense camera model used a similar techno...
-
Hi Hisatsugu Horiuchi Thanks very much for your questions. 1. The D455 camera model has a minimum depth sensing distance of around 0.5 meters / 50 cm. When objects are nearer to the camera tha...
-
There is not an official explanation for this very rare failure, so I would not want to speculate about RealSense cameras specifically. In general though, certain storage conditions might lead to c...
-
Some manufacturers of products in general - not Intel in particular - will have an 'acceptable failure rate', a small percentage of the total units shipped from the factory that will already be dea...
-
The Intel RealSense Help Center's official guidance article about returns can be found at the link below. https://support.intelrealsense.com/hc/en-us/articles/360051623953-How-to-return-a-faulty-In...
-
Hi Arthur Levisalles10 What kind of pointcloud image do you get if you use the RealSense SDK's Python example script opencv_pointcloud_viewer.py https://github.com/IntelRealSense/librealsense/blob...
-
If a camera works normally and then suddenly stops working overnight, another possible cause is that Windows has installed an update that conflicts with the camera. This has happened a number of t...
-
Hi Ian Oberdorf If you are using Windows then each individual RealSense camera has its own pair of depth and RGB drivers installed on the computer. So if you have two D415 then there will be 2x t...