MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
The documentation for rs-kinfu states that OpenCV 4 is required (not a suggestion), so I would recommend OpenCV 4.
-
The D457 can be used with the RealSense library on a GMSL cable connection from version 2.53.1 onwards. To make it work with a desktop PC, you will need to convert ("port") the MIPI driver for us...
-
Hi, there is not assistance available for debugging errors that occur when running rs-kinfu, unfortunately. The first step in diagnosing problems with rs-kinfu is to comment out the line of rs-ki...
-
Hi Marocharoma For the application of scanning hand surface geometry, the data transfer speed provided by a GMSL/FAKRA connection would be unnecessary. Your latency problem may be due to the D4...
-
Instead of splicing (or "stitching" separate front and back pointcloud scans together, you could consider using the RealSense SDK example program rs-kinfu. With this program, you can move a single...
-
Hello, you may find helpful a guide at the link below for creating a 'point cloud' scan with the RealSense Viewer tool and then converting it into a solid object .obj file using a free tool called ...
-
You are very welcome. It's great to hear that you achieved a solution through the Python SDK. Thanks very much for the update!
-
The L515 is a retired camera model and is no longer supported in the RealSense SDK and RealSense Viewer. The D455 that you currently have has a wide field of view size and your crate is only jus...
-
After you perform a calibration, are you writing it to the camera hardware and exporting an xmil file after every calibration using the command below? Intel.RealSense.CustomRW.exe -w -f myfile.xml ...
-
Looking at the area in the bottom where the shaking is worst and looking at the same area on the RGB mage, the dark gray area there might be contributing to the instability. It is a general physic...