MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
All of the AmazonBasics powered models are listed as currently unavailable, unfortunately. I do not have a list of other hubs that are confirmed to work with RealSense, though of course AmazonBas...
-
I recommended the AmazonBasics powered hub in a comment above. Thanks very much for the confirmation of the firmware version.
-
Amazon's own-brand powered hub AmazonBasics works excellently with RealSense cameras. Intel used a 4-port one in 2018 for testing camera data bandwidth at the link below. https://dev.intelrealsen...
-
If you have the camera plugged directly into a USB port on the Lenovo then you could try plugging the camera into a USB hub instead. This would confirm whether or not the problem is related to the...
-
Thanks very much for the information. What computer or computing device are you using the camera with, please? Is it a full computer such as a desktop or laptop PC, or a single-board computing ...
-
Hi Pim Bakker Your camera should be able to sustain a cable connection on a high quality Newnex cable with active repeater components to maintain the signal strength over distance. Which version...
-
For OpenCV camera calibration questions, the best Python / OpenCV reference that I know of is the tutorial at the link below. https://docs.opencv.org/4.x/dc/dbb/tutorial_py_calibration.html I do ...
-
The downside of Disparity Shift is that whilst increasing it above 0 reduces the minimum depth distance, increasing the value also progressively reduces the maximum observable depth range and strip...
-
Hi Dorus Van Dintherly The best solution may be to define and apply a fixed set of manually defined coefficient values i a script instead of using the camera's intrinsics, to provide a 'one size f...
-
Hi Liam Neric The problem with the D455 depth image seems to occur with the depth nearest to the camera. the D435 has a minimum depth sensing distance of around 0.15 meters, whilst D455's minimum...