MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
H Valay Patel The rs-grabcuts RealSense OpenCV example program may provide some useful insights if you have not seen it already. It creates two masks, a near one and a far one. https://github.com...
-
If you are using an RGB color image then I would recommend increasing the Sharpness RGB option to its maximum value of '100' for best RGB image clarity. Also, if you are using the depth or infrar...
-
Once the camera has become inoperable then there is no way for customers to update the firmware again to fix it because the camera cannot be accessed. If the camera was purchased less than 30 days...
-
Support for the D455 model was not introduced until 2.38.1. It sounds as though the 2.35.2 RealSense Viewer has installed a version of the camera firmware driver that is very old. D455 works w...
-
Has the camera always had this problem since the first time that you purchased it?
-
Thank you. Does the error still occur if you unplug the micro-sized USB cable connector from the bottom of the D455 camera, turn the connector around the other way and plug it back in please? USB...
-
Hi Maxxxcim What is the name of the error that occurs, please? Where does the error happen? For example, when the camera is plugged in when using the RealSense Viewer tool?
-
Hi Duke Zacks The camera should be calibrated for underwater use instead of the usual use in atmospheric air. The best available technical discussion about underwater calibration is at the link ...
-
Thanks very much for the update. I recommend contacting Newnex through their support page to explain your problem. https://newnex.com/technology-support.php
-
Hello, thanks for your question. In the 3D view in the above image, red is X (horizontal), green is Y (vertical) and blue is Z (forward, which is distance / depth).