MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
When the D4 V3 board is used with D430, it should give the configuration of 'D430i' (a camera that has an IMU sensor but does not have an RGB sensor). The RGB sensor is sensor '1' and in the D435 ...
-
Calibration can provide information about the general quality of the camera's calibration but not the accuracy of specific coordinates.
-
Hello, a method of checking the accuracy of the camera is to use the RealSense SDK's Depth Quality Tool and point the camera at a wall, then look in the program's options side-panel for a value cal...
-
Although the ideal depth sensing range of the D405 is 7 to 50 cm, it can render depth that is up to a couple of meters away. The camera would not be able to read the depth of the tire tread groove...
-
Hi Himanshu Pradhan A suitable RealSense camera model for this application would be one that has excellent accuracy and image quality at close / very close range. The RealSense D405 would fit tho...
-
You are very welcome. Thanks very much for the information!
-
It is a last-resort method to explore if communication with the place that you bought an item from fails to provide a satisfactory outcome.
-
-
If the camera was not purchased from Intel's official RealSense Store, the description of the condition of the camera and its box opens the possibility that the camera was previously returned as fa...
-
Hi Joshuakery1 If the camera has just been purchased brand new from a retailer and just taken out of the box then it should not have experienced long-term storage inactive conditions that would le...