MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Yes, the libuvc backend procedure would require reinstalling librealsense. I would definitely recommend uninstalling the previous one first. You should be able to uninstall and reinstall by goin...
-
For anyone else who reads this discussion in future who has a D435f / D435if or D455f, they should not downgrade their firmware to 5.13.0.50 or their camera will become undetectable. Firmware 5.15...
-
I'm pleased to hear that the camera works fine on Windows. This demonstrates that the camera has not had a firmware installation failure that prevents the camera from operating. Because the firm...
-
Have you tested the D435i's IMU recently to see whether it was working correctly before this firmware update occurred? I ask this because I note that the error message refers to not being able to ...
-
https://dev.intelrealsense.com/docs/firmware-releases-d400#d400-series-firmware-downloads
-
Thank you. It is recommended that firmware updates are performed with the 1 meter official cable if possible rather than a long cable of your own choice. Firmware 5.16.0.1 is correct for use wit...
-
Hi Happydrones123 Which version of the RealSense SDK / RealSense Viewer are you using, please? Are you using the official 1 meter long USB cable supplied with the camera or a cable of your own c...
-
Hi Prarthana Sigedar The all-blue color indicates that the wall and the cups are at approximately the same distance from the camera. By default, depth is represented by color values that shift be...
-
Yes, 850 nm is the wavelength. As far as I can tell, the API instructions for 57 and 91 frequency (RS2_EMITTER_FREQUENCY_57_KHZ and RS2_EMITTER_FREQUENCY_91_KHZ) have not appeared anywhere outs...
-
Hi Jdzitsiuk The IR projector operates at around 850 nm. RealSense 400 Series cameras do not interfere with each other, but they can interfere with non-RealSense devices nearby that use IR. The ...