MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Hi Mmaniacco A single specific frame cannot be exported from a bag file using the rs-convert tool, unfortunately. It is possible to export IMU data to a .csv log file using the rs-data-collect.C...
-
Going back over this case, I note that images from the '2D' mode of the RealSense Viewer are being compared with ones from the '3D' mode. It is normal for the image to have less detail and more ho...
-
Hi Eliezerjustin4 The DKMS packages at the distribution_linux.md page are designed for use on PCs. When installing for Ubuntu on Raspberry Pi, it is recommended to build the SDK from source code ...
-
Thanks very much for the information. Firmware version 5.16.0.1 is the appropriate one to use with SDK 2.55.1. SDK 2.49.0 was designed for use with firmware 5.12.14.50. However, if a D455 is ...
-
Hi Steve Steve There have not been past reports of camera disconnection due to USB cables being exposed to static electricity. However, when multiple RealSense cameras are connected together with...
-
Hi Steve Steve RealSense cameras are calibrated in the factory and so are normally very well calibrated when new out of the box after purchase. Events that could cause a miscalibration include a...
-
Hi Gw Lee Which firmware driver version do you have installed in your camera, please? You can find the firmware version by clicking on the Info button at the top of the RealSense Viewer's options...
-
Hi Sjkimy Thanks very much for your contact. I will send you an email to introduce myself.
-
RealSense support for Java took two separate forms: the official Android wrapper, and an unofficial non-Android Java wrapper that a RealSense community member developed. https://github.com/edwinRND...
-
Hi Yixun Liu A RealSense Java script at the link below demonstrates accessing intrinsics with the get_intrinsics instruction. https://jar-download.com/artifacts/org.bytedeco.javacpp-presets/librea...