MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
It looks like the errors start after logging into the ethernet network is initiated. Have you (1) logged into the remote NUC from your main 'host' PC using an SSH connection; and then (2) configu...
-
Please try inputting the command below into the Ubuntu terminal to install the udev rule, which handles devices such as RealSense cameras. sudo cp ~/.99-realsense-libusb.rules /etc/udev/rules.d/99-...
-
-
If you need to build 2.51.1 from source code then the best approach would be to use the RSUSB backend installation method. Please follow the instructions below, but use the source code file for 2....
-
It is okay to use a NUC as the 'remote' computer that the camera is attached to instead of a Pi so long as the NUC is using Ubuntu as its OS. 18.04 would be fine.
-
If using SDK 2.51.1 then the recommended camera firmware version to use is 5.13.0.50. This is the absolute minimum firmware that supports D405 and you should not install an older firmware than 5.1...
-
If you are able to access the Euclid then the discussion below describes how to initiate the 'new out of the box' OOBE (Out Of Box Experience) initial setup process in the terminal. https://communi...
-
If you wish to replicate the Euclid's ability to be signed into over a web interface then the interface can be compiled at the repository below. https://github.com/IntelEuclid/euclid_web_ui
-
Hello, I searched extensively for a surviving Intel Euclid factory image but was unable to locate one, unfortunately. Euclid was a candy bar sized miniature PC equipped with a RealSense ZR300 ste...
-
As official D405 support was introduced in SDK 2.51.1, that means that 2.51.1 is the only networking-supporting version older than 2.53.1 that would likely work correctly with D405.