MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Whilst I do not have much data on real-world operating temperatures of the ASIC, 41 degrees is consistent with readouts that have been provided in the past by other users of the 400 Series cameras ...
-
Raspbian is based on the 'Debian' form of the Linux OS. Page 15 of the user guide for the calibration tools describes how to install the calibration tools package for Debian. The CustomRW program...
-
There is an indirect way to get to the Troubleshoot from the Control Panel's front page in Windows 10. STEP ONE Open the 'System and Security' section STEP TWO Under the 'Security and Maintenance' ...
-
DSO numbers are related to Intel's internal bug tracking system. As the DSO numbers never have clickable links, it is hard to find out information about them. Are you using sync cables to synchron...
-
I would not expect the T265 to work with the RSSDK SDK or cameraviewer.CPP.exe, as the old SDK from 2016 was created years before the T265 existed and does not support modern RealSense cameras (the...
-
Other T265 users have experienced this issue of non-detection and the listing of the device as Movidius. My understanding is that with the T265, it differs from the RealSense depth cameras in that ...
-
Problems with detecting the T265 sometimes is a known issue. For example, if using the T265 with a USB hub, it is recommended that the USB hub is powered up first and then the T265 is connected to...
-
The release notes for the RealSense SDK say that Android is not supported yet on D435i, unfortunately.
-
Sometimes the RGB driver is placed by the computer in the 'Camera' section of the Device Manager instead of in Imaging Devices with the other drivers. So there can be differences in the driver loc...
-
It should be possible to display the monochrome fisheye cameras in the Viewer, yes. https://www.youtube.com/watch?v=9f8qoTuR_I4 I have not actually used a T265 myself. My understanding is that the...