MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
We are at the point where it may be necessary to start considering trying the alternative Python-based EtherSense ethernet networking tool that is the predecessor of rs-server and is still supporte...
-
In regard to the list of Invalid Options (which are all related to RGB color), this may be because the D405 model is not equipped with an RGB sensor component (it obtains its RGB image from the dep...
-
If the network connection to the remote camera has been successfully established then it should be listed in the side-panel of the Viewer as a Network Device, like the image below from the networki...
-
Hi Yasodeafs The RealSense D435 camera model is likely to meet your requirements, as long as the person is standing 1.5 meters or more from the camera. Its field of vision is wide enough to captu...
-
Ok, thanks very much for testing the pre-made 2.51.1 Viewer. I got the same message when I just tried that Viewer myself. The 2.50.0 version of the Viewer does seem to have the network function ...
-
The Windows instructions recommend downloading and running the pre-made version of the RealSense SDK / RealSense Viewer available on the SDK Releases page rather than compiling it yourself from sou...
-
I suspect that the username in the documentation is only realsense because that's how the Pi SD card image was configured.
-
-
-