MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Hi Bhagwatok Yes, it is fine to mount RealSense cameras pointing vertically downwards and usually it should not have a negative effect on depth measurement accuracy. However, measuring a box on a...
-
In the D457 camera product, almost everything needed to set it up on a FAKRA GMSL cable connection, including the FAKRA GMSL connector and hardware sync pins, is built into the camera. It will be...
-
Hi Grzegorz Bartosz Yes the part number 82635DSD457 is the Product Code for a single D457 camera. If they want a multi-pack of the camera then MP is added onto the end of the code.
-
Also, are your slave cameras set to Inter Cam Sync Mode '2' (slave) or to Mode 4 (genlock slave). If you are using mode 2, you could try setting the slaves to 4 to see how it affects performance. ...
-
How long are your hardware sync cables, please? If they are longer than 3 meters then static could build up and then discharge, causing a camera's frame counter to reset unless the cable has had c...
-
If the sensors were being affected by strong light then defining a Region of Interest (ROI) in the lower half of the image or applying an external Neural Density (ND) filter - such as the CLAREX NI...
-
Hi Bschwartz I count 21 cameras on your image, all apparently attached to the same computer. Even if there is enough data bandwidth for the cameras, each attached camera will consume a portion of...
-
If the 'closer to zero the better' principle of the On-Chip calibration also applies to Tare (the documentation does not state this) then if the old calibration was 0.0570 and the new calibration w...
-
I am not familiar with this Tare health check, though clearly Tare does have its own score and so I have edited my earlier comment to reflect this. My apologies for the confusion. The calibratio...
-
0 to 0.25 is Good. 0.25 - 0.75 is Could Be Improved. 0.75 and above is Needs Recalibration. So you are just on the edge of the need for improvement.