MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
One possible option would be to use two cameras and arrange them in a vertical stack in an upper and lower arrangement. This would widen the vertical field of view considerably so that the camera ...
-
An official CAD model file for the RealSense SR305 is now available if you should require it. https://dev.intelrealsense.com/docs/cad-files
-
Your robot concept is similar to Tally, a retail inventory robot using open-source tech that combines lidar with RealSense. So it is a good reference source for working out your own design. https:...
-
You could try turning the Laser Power setting down to see if it reduces the temperature. The depth sensing should still function. If that does not make a difference then you have realistically do...
-
Are you able to try the D435i with a different USB-C cable please to eliminate the possibility that the heating is caused by the USB cable? If you are getting the same results on different machines...
-
From the reports I have seen on the internet about rapid heating of USB devices (not just RealSense), I would expect the casing to become hot within the first few minutes of operation.
-
I just recalled that a faulty USB cable can also cause the rapid overheating problem with USB devices. Since the D435i and SR305 use different cable types, this may be why the SR305 does not exper...
-
It would be the USB port at the computer end, not the camera's port. If other USB devices such as the SR305 are not rapidly heating up, that may indicate that the port is okay and it is an issue sp...
-
It is definitely a highly abnormal temperature for those conditions. One effect of excessive temperature could be the disruption of the camera's calibration, requiring a re-calibration of the came...
-
LED lights should be the best type of lights to use - better than ordinary bulb lights - because they do not cast shadows on the scene. That is why LED lights are used in professional photography....