MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Hi Gunjinageswarrao0 You are unlikely to be successful with this goal on a Raspberry Pi 4, unfortunately. When using a RealSnse camera with a Raspberry Pi 4, performance is limited and the best t...
-
-
Some RealSense users have also successfully used Isaac ROS Visual SLAM, a tutorial for which is here: https://nvidia-isaac-ros.github.io/concepts/visual_slam/cuvslam/tutorial_realsense.html#tutoria...
-
Hi Konyaa I ran tests on a few curved objects that were approximately 4 mm wide and 1 meter (1000 mm) long and made of different materials, using various RealSense camera models (D405, D415, D435F...
-
The IMU measures acceleration in the unit meters per second squared (m/s²) and gyroscopic angular velocity is measured in the unit radians per second (rad/s). So the acceleration already takes acc...
-
Hi Allusrikanth87349 The D455's IMU motion-tracking hardware component contains an accelerometer that can provide x, y and z velocity values. This information can be accessed using programming co...
-
Yes, you can use the USB-C port instead of the GMSL FAKRA connector. In this mode, the camera will be detected as a D455 and behave and perform exactly like one. To enable the USB connector, a re...
-
Hello, the company Leopard Imaging provide a deserializer module that is compatible with D457, though it is currently listed as out of stock at the time of writing this. https://leopardimaging.com/...
-
Thanks very much for the update. The multi-camera guide has electronics blueprints for adding anti-ESD components to the sync cable if you want to test whether static due to cable length is the ca...
-
Hi Onkar It should not be necessary to adapt the box_dimensioner_multicam project for use with a single camera as, despite the project's name, it can work fine with a single camera placed at the c...