MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Intel has published a guide to using a T265 and depth camera together, which includes a section on the benefits of this pairing for scanning and 3D reconstruction. https://www.intelrealsense.com/de...
-
The ideal situation for simplicity is to have a single pipeline. It is possible to have multiple threads, but if you are only using one device (the T265) instead of multiple devices then it is lik...
-
A member of the Intel RealSense team on the GitHub site gave the advice below to a user with the same error: "The specific error appear when the application tries to configure stream with unsupport...
-
Apologies for the delay in responding further, as I was considering your question carefully. I do not have a T265 here with me, so cannot conduct my own tests. Can you try toggling off the 'GLSL S...
-
The conversation in the link below discusses user reports of pose drift when using the T265 with USB2 connections. The users found that there tended to more often be drift problems when using ROS ...
-
I thought about your question very carefully. The use of OpenCV and imwrite / imshow means that it goes outside of my programming knowledge, unfortunately. The best place to get expert advice on...
-
The RealSense D435i camera would be the best choice, as it works well outdoors, has a wide field of view and a fast shutter suited to tracking fast moving objects. You can widen the view further b...
-
When using the camera at very close range to an object, reducing the depth unit value can improve accuracy. On the 400 Series cameras, the default depth unit value (the one under the Controls opt...
-
You are very welcome. Good luck, and please return here any time if you have further questions.
-
For the D435, the optimal resolution is 848x480. If you would like to achieve a higher quality image, the D415 model is better suited to scanning a small, non-moving object. It has around 2.5x th...