MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
The accelerometer and gyro readings will be local to the IMU that is generating them inside the T261. So having two cameras vertically stacked should not affect the gyro readings, since one camera...
-
I could not find any references to saving a MATLAB cloud unfortunately. The best course of action will be to enquire at the RealSense GitHub forum by visiting the link below and clicking on the N...
-
I hope that the discussion in the link below will be helpful to you. https://github.com/IntelRealSense/librealsense/issues/2576
-
I am not on the Intel developer or engineer team, so a member of those teams will be better able to tell you about how RealSense handles ground truth. You can enquire to them by visiting the Real...
-
It looks as though the document is suggesting that a laser rangefinder or tape measure are methods by which people can calculate ground truth, but the camera itself does not do the full ground trut...
-
The depth accuracy of the D400 series cameras is less than one percent of the distance from the object. So if the camera is 1m from the object, the expected accuracy is between 2.5mm to 5mm. The ne...
-
That's great news. Thanks for the update!
-
You are welcome. I'm pleased that the GitHub was able to help you!
-
When cameras are mounted vertically in close proximity to one another, they are typically pointing straight ahead. By crossing the laser beams over by tilting the upper camera down and the lower c...
-
If the camera is working fine on the Jetson Nano then the problem is probably not related to the firmware driver. The firmware is stored inside the camera and not on the PC, so any problem with th...