MartyG
- Total activity 5964
- Last activity
- Member since
- Following 0 users
- Followed by 7 users
- Votes 3
- Subscriptions 1820
Comments
Recent activity by MartyG-
Your Intel graphics should work fine with the camera. Do you use Windows 10? If so, have you downloaded and installled the full 750 mb RealSense SDK please?
-
You are very welcome. :) PLY files are recordings of 3D point cloud data, yes.
-
The .STEP files on the CAD (Computer Aided Design) page are not camera data recordings. They are 3D models of RealSense camera products with precisely correct measurements. STEP files can be used...
-
Using the "Default" preset will give best visual appeal, clean edges and reduced point cloud spraying. Using a high resolution will also improve accuracy - the optimal depth resolution for the D41...
-
There is nothing that I can do as a support person to influence the design of the website. I will pass a link to this discussion to a senior manager at Intel Support who takes user-interface desig...
-
The RealSense Viewer has a range of post-processing filters enabled by default that improve the image quality. These can be found in the Post-Processing section of the options at the side of the R...
-
A CAD file for the L515 is not available yet. When it is, it should be on the CAD file page at the link below. https://dev.intelrealsense.com/docs/cad-files In the meantime, it is possible to get...
-
Hello again Richard! You can submit feedback about the website by visiting the contact form at the link below and choosing the "Site Related" option from the 'Please Select a Topic' drop-down menu....
-
The cost of the OEM Target Board is mostly the cost of manufacturing the physical board. As far as I know, the only other way to get the OEM software is if you have a Non Disclosure Agreement (NDA...
-
T265 questions are now being handled on the RealSense GitHub forum. Please re-post your question there by visiting the link below and clicking on the 'New Issue' button. I apologise for the inco...